Breadcrumb Home EVERY GRID STABILITY CHALLENGE. ONE PARTNER. The energy transition is rewriting the rules of grid operation. As synchronous generation retires and inverter-based resources take its place, grid operators face stability challenges that traditional tools were never designed to solve. GE Vernova's grid stability portfolio delivers proven, scalable solutions for every stage of the energy transition. Talk to a Grid Stability Expert The Grid Is Changing. Is Your Stability Strategy Keeping Up? Today's power grid is undergoing its most profound transformation in a century, and the pace is accelerating.The rapid growth of renewable energy, the retirement of conventional thermal generation, and the rise of inverter-based resources (IBR) are collectively eroding the physical properties grids have always relied on: inertia, fault current, and reactive power support. These are not future risks. They are present-day operational realities.The consequences are compounding. Frequency excursions are harder to arrest. Voltage fluctuations are more frequent and less predictable. Transmission corridors are congested while new infrastructure takes years, sometimes decades, to permit.GE Vernova's grid stability portfolio is built around five defining challenges of the energy transition, with a clear solution pathway from foundational capability to fully integrated, advanced architectures. XX Projects Delivered XX Countries Served XX Years Experience Five Challenges Defining Grid Stability Today The critical grid stability challenges operators are navigating right now, and the solutions GE Vernova has built to address them. 1 Inertia Loss and Grid-Forming Capability 2 Transmission Congestion and Power Flow Control 3 Voltage Instability and Reactive Power Management 4 High IBR Penetration and Low Short-Circuit Ratio Grids 5 Islanded and Remote Grid Stability Inertia Loss and Grid-Forming Capability As inverter-based resources replace synchronous generators, the grid is losing the physical inertia that once buffered against frequency disturbances. Without adequate inertia, even minor generation-load imbalances can trigger rapid frequency deviations, leaving operators with less time to respond and greater risk of cascading events.Modern power systems require grid-forming technology capable of synthesizing inertia-like behavior and providing stable voltage and frequency references in IBR-dominated systems.GE Vernova's grid-forming solutions range from GFM STATCOMs for foundational IBR-heavy environments to fully integrated GFM BESS plus synchronous condenser architectures delivering physical inertia, grid-forming control, and black start capability in a single system.Explore Grid-Forming SolutionsGFM STATCOMGFM IBR with BESSGFM BESS plus SYNCON Transmission Congestion and Power Flow Control Generation capacity alone cannot solve an energy transition constrained by transmission infrastructure. Across many regions, low-cost renewable generation is effectively stranded. Transmission corridors are congested, unevenly loaded, or operating well below capacity. Building new lines is a decade-long endeavor that is simply not a viable near-term option for most operators.Flexible AC Transmission System (FACTS) technology offers a faster, more cost-effective path, unlocking additional capacity across existing infrastructure without waiting for new construction.GE Vernova's power flow solutions span from Fixed Series Compensation (FSC) for proven flow improvement, to the FSC plus SSSC hybrid for dynamic control and oscillation damping, to the Unified Power Flow Controller (UPFC) for maximum network flexibility.Explore Power Flow Control SolutionsFSCFSC + SSSC HybridUPFC Voltage Instability and Reactive Power Management As synchronous generators are displaced by inverter-based resources, dynamic reactive power reserves are declining across networks worldwide. The result is a grid increasingly susceptible to voltage fluctuations, power quality degradation, flicker, and in severe cases, voltage collapse.Reactive power cannot be transmitted efficiently over long distances, making local, fast-responding compensation essential. Grid operators need solutions that inject or absorb reactive power dynamically and respond within milliseconds.GE Vernova's voltage stability solutions scale to grid complexity, from ESTATCOM systems for fast precise dynamic support, to GFM STATCOMs for demanding grid environments, to GFM BESS plus synchronous condenser architectures for the most complex network conditions.Explore Power Flow Control SolutionsESTATCOMGFM STATCOMGFM BESS plus SYNCON High IBR Penetration and Low Short-Circuit Ratio Grids In power systems with high inverter-based resource penetration, two related problems emerge simultaneously: fault current levels decline and short-circuit ratios (SCR) fall. Both trends undermine the assumptions behind conventional grid protection and stability architectures.Low SCR environments, sometimes called weak grids, are prone to voltage instability, control interactions between IBR devices, and sub-synchronous oscillations. As IBR penetration grows globally, these conditions are becoming mainstream operational challenges, not edge cases.GE Vernova's solutions for high-IBR, low-SCR environments range from GFM STATCOMs providing foundational short-circuit support to integrated GFM BESS plus synchronous condenser systems delivering maximum short-circuit strength, grid-forming capability, and physical inertia in a single architectureExplore Power Flow Control SolutionsGFM STATCOMSYNCON plus ESTATCOMGFM BESS plus SYNCON Islanded and Remote Grid Stability Not every grid has a large interconnected system to rely on. Remote microgrids, island power systems, and isolated industrial networks must independently form voltage and frequency references, sustain stable operation under variable load, and restore service after outages with no external support available.These environments represent the most demanding test of modern grid stability technology. There is no inertial backup from neighboring systems, no large generation pool to absorb disturbances, and no margin for instability.GE Vernova addresses the full spectrum of islanded grid challenges, from condensed inertia and black start solutions for standalone environments to fully integrated GFM BESS plus synchronous condenser architectures for the most demanding standalone systems.Explore Power Flow Control SolutionsGFM STATCOMSYNCON plus ESTATCOMGFM BESS plus SYNCON GE Vernova's grid stability portfolio spans foundational to advanced architectures, addressing inertia loss, transmission congestion, voltage instability, high IBR penetration, and islanded grid operation. Download the Portfolio Overview Featured Resources Explore integrated grid stability solutions—from FACTS and grid-forming technology to advanced orchestration—to navigate inverter-based resources, transmission congestion, and evolving grid challenges. Download Stability Whitepaper Explore the role of FACTS technology in maximizing existing network capacity to solve congestion challenges and support the rapid pace of the global energy transition. Download FACTS Whitepaper 2 / 2